Information booklet

Information to the shareholders of AB SKF regarding redemption of shares 2008

Read more about the proposed redemption of shares 2008 in the information booklet below.

Information booklet (pdf)

Information to the shareholders of AB SKF regarding redemption of shares 2007

No action needs to be taken on behalf of the shareholders in SKF in order to receive the payment of the redemption amount as the redemption procedure is automatic.

Please note that for shareholders with a limited tax liability in Sweden (principally shareholders that are domiciled outside of Sweden), Swedish withholding tax will not be payable if the redemption shares are sold in the market during the period May 21, 2007 to June 7, 2007, inclusive. Swedish withholding tax will, however, be payable if the redemption shares are not sold in the market but instead redeemed by SKF.

Read more in the information booklet below.

Information booklet (pdf)

Information to the shareholders of AB SKF regarding proposed split and redemption of shares 2005

Read more about the proposed split and redemption of shares 2005 in the information booklet below.

Information booklet (pdf)

 

SKF logo